LX2160A Processor Errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A Processor Errors

Jump to solution
875 Views
bboykaz
Contributor I

Hi, 

LX2160ARM.pdf specifies ORed error interrupts from processor clusters as Interrupt IDs 96...103. 

Where can I find a list of errors which are ORed in these interrupt?

Thanks.

0 Kudos
Reply
1 Solution
804 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

each interrupt ID corresponds to a cluster,

the LX2160A has a Sixteen 32-bit/64-bit Arm v8 A72 CPUs arranged as clusters of two cores sharing a 1 MB L2 cache, it means if there is any error on one core the assigned cluster will trigger the corresponding interrupt, those interrupts are ORed and connected to GIC at the mentioned ID slots, for more information about the interrupts you can refer to the ARM GIC manual.

View solution in original post

0 Kudos
Reply
1 Reply
805 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

each interrupt ID corresponds to a cluster,

the LX2160A has a Sixteen 32-bit/64-bit Arm v8 A72 CPUs arranged as clusters of two cores sharing a 1 MB L2 cache, it means if there is any error on one core the assigned cluster will trigger the corresponding interrupt, those interrupts are ORed and connected to GIC at the mentioned ID slots, for more information about the interrupts you can refer to the ARM GIC manual.

0 Kudos
Reply