LTIB with iMX25 / Bad md5 for udev-117-imx-lowcase2.patch / Missing file on GPP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTIB with iMX25 / Bad md5 for udev-117-imx-lowcase2.patch / Missing file on GPP

Jump to solution
3,682 Views
Apple92
Contributor II

Hi,

 

I am generating a kernel by using LTIB configured for iMx35 3-Stack board.

 

There happens a weird error.  When building udev, LTIB tries to patch a file.

nevertheless, the patch file md5 mismatches the MD5 value in the patch.md5 file.

Thus, LTIB renames the file with the bad extension and stops. I launch again

./ltib and LTIB tries to connect to the GPP on bitshrine server. The issue is that

this file does not exist on the current GPP. This file is udev-117-imx-lowcase2.patch

whereas udev-117-imx-lowcase.patch (yes, the same without the "2") exists !

 

Did someone face the same issue?

 

here is the script extracted from the error output.

 

Processing: udev

==================

Build path taken because: no prebuilt rpm,

ERROR: md5sum mismatch, re-naming /opt/freescale/pkgs/udev-117-imx-lowcase2.patch to /opt/freescale/pkgs/udev-117-imx-lowcase2.patch.bad, please re-try

Can't get: udev-117-imx-lowcase2.patch at ./ltib line 786.

 

 

f_buildrpms() returned an error, exiting

traceback:

main:557

 

 

Started: Wed Sep 16 18:16:16 2009

Ended: Wed Sep 16 18:16:17 2009

Elapsed: 1 seconds

 

These packages failed to build:

udev

 

Build Failed

 

Exiting on error or interrupt

 

 

 

Second launch:

 

Processing: udev

==================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

 

Try udev-117-imx-lowcase2.patch from the GPP

http://bitshrine.org/gpp/udev-117-imx-lowcase2.patch:

18:17:33 ERROR 404: Not Found.

Can't get: udev-117-imx-lowcase2.patch at ./ltib line 786.

 

 

f_buildrpms() returned an error, exiting

traceback:

main:557

 

 

Started: Wed Sep 16 18:17:30 2009

Ended: Wed Sep 16 18:17:33 2009

Elapsed: 3 seconds

 

These packages failed to build:

udev

 

Build Failed

 

Exiting on error or interrupt

 

Regards,

Apple92

 

0 Kudos
Reply
1 Solution
1,781 Views
Apple92
Contributor II

Finally, there are still bad MD5 files in the package shipment. I computed them with md5sum commands and now the build chain is OK.

 

Thus, if you use Freescale iMX35 CD, check the MD5 files and compute them yourself if you want to have clean source files.

 

Regards

View solution in original post

0 Kudos
Reply
2 Replies
1,781 Views
Apple92
Contributor II
Frescale tech support sent me modified files. I am testing this and will set the topic to [SOLVED] if this works fine now.
0 Kudos
Reply
1,782 Views
Apple92
Contributor II

Finally, there are still bad MD5 files in the package shipment. I computed them with md5sum commands and now the build chain is OK.

 

Thus, if you use Freescale iMX35 CD, check the MD5 files and compute them yourself if you want to have clean source files.

 

Regards

0 Kudos
Reply