LS1046A RDB mbed serial drive not connecting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A RDB mbed serial drive not connecting

Jump to solution
3,706 Views
balaka
Contributor III

while setup my LS1046A RDB board frist time and followed the Getting Started Guide:

Downloaded and installed the mbed serial port driver and installed Tera Term,

When connecting the USB cable between console port and PC, Windows shows an USB drive/folder for a short period, and then disappears. This continues on and on. The green LED D8 periodically blinks (like the CMSIS-DAP controller is rebooting).

Host machine is having the windows 11.

0 Kudos
Reply
1 Solution
3,624 Views
balaka
Contributor III

This step :

This is the workaround we have confirmed to fix the mbed issue on Win10 PC's:
- Go to the "Start" option on the PC and type the command "Services"
- Than you should see the following "Services" window open
- Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"

I tried before posting the issue here.

Now I try to follow the steps in https://os.mbed.com/blog/entry/DAPLink-bootloader-update/

but i am not allowed to copy the file k22fx512_if_mbed.bin to the BOOTLOADER Drive.

View solution in original post

0 Kudos
Reply
7 Replies
3,673 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the attached document and MBED firmware image (in the ZIP package).

There is a known issue with MBED operation under Win10(Could be the same for Win11):
https://os.mbed.com/blog/entry/DAPLink-bootloader-update/

This is the workaround we have confirmed to fix the mbed issue on Win10 PC's:
- Go to the "Start" option on the PC and type the command "Services"
- Than you should see the following "Services" window open
- Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"

0 Kudos
Reply
3,636 Views
balaka
Contributor III

Following the steps given in 

DAPLink bootloader update | Mbed

But to od the step 3 it is not allowing the BOOTLOADER drive to copy the image inside.\

 

Could you please suggest?

0 Kudos
Reply
3,616 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please try in a Win10 Machine and share your result.

0 Kudos
Reply
3,573 Views
balaka
Contributor III
I tried with the windows10 also. when we drag and drop the k22fx512_if_mbed.bin file.
Geeting the error
"You need permission to perform this action"
0 Kudos
Reply
3,544 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please send images of the process you followed and the permission error.

0 Kudos
Reply
3,502 Views
balaka
Contributor III
this is issue due to write permissions not available in USB.
0 Kudos
Reply
3,625 Views
balaka
Contributor III

This step :

This is the workaround we have confirmed to fix the mbed issue on Win10 PC's:
- Go to the "Start" option on the PC and type the command "Services"
- Than you should see the following "Services" window open
- Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"

I tried before posting the issue here.

Now I try to follow the steps in https://os.mbed.com/blog/entry/DAPLink-bootloader-update/

but i am not allowed to copy the file k22fx512_if_mbed.bin to the BOOTLOADER Drive.

0 Kudos
Reply