LS1027A PORESET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1027A PORESET

1,708 Views
JOM_alor
Contributor I

Hi,

I am designing a CPU based on the LS1027A. In the reference manual LS1028ARM (Table 12) is defined the power-on sequence for that device. The question is related with the initial stages and PORESET.

Is it necessary to perform a full PORESET pulse (falling and rising edge) or is it enought to mantain PORESET low more than 1ms after all power rails are ok and then rise it to '1'?

If the second option is possible it is easy to do that with a voltage monitor.

 

Thanks in advance.

0 Kudos
Reply
3 Replies

1,699 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @JOM_alor,

The PORESET_B signal should be asserted for atleast 1ms after all the supply rails are stable.

Regards,
Mrudang

0 Kudos
Reply

1,695 Views
JOM_alor
Contributor I

Hi,

OK. But the question is: should I assert PORESET_B with a "full" assertion pulse (1 ==> 0 ==> 1) or can I mantain PORESET_B al low level from power-supply startup and after at least 1ms deasset it (0 ==> 1)?

Many thanks for your fast answer!

 

0 Kudos
Reply

1,682 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @JOM_alor,

The PORESET_B signal must be low till the all the supplies are stable which means there will be 0==>1 logic.

Regards,
Mrudang

0 Kudos
Reply