LS1027A PORESET

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1027A PORESET

1,689件の閲覧回数
JOM_alor
Contributor I

Hi,

I am designing a CPU based on the LS1027A. In the reference manual LS1028ARM (Table 12) is defined the power-on sequence for that device. The question is related with the initial stages and PORESET.

Is it necessary to perform a full PORESET pulse (falling and rising edge) or is it enought to mantain PORESET low more than 1ms after all power rails are ok and then rise it to '1'?

If the second option is possible it is easy to do that with a voltage monitor.

 

Thanks in advance.

0 件の賞賛
返信
3 返答(返信)

1,680件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @JOM_alor,

The PORESET_B signal should be asserted for atleast 1ms after all the supply rails are stable.

Regards,
Mrudang

0 件の賞賛
返信

1,676件の閲覧回数
JOM_alor
Contributor I

Hi,

OK. But the question is: should I assert PORESET_B with a "full" assertion pulse (1 ==> 0 ==> 1) or can I mantain PORESET_B al low level from power-supply startup and after at least 1ms deasset it (0 ==> 1)?

Many thanks for your fast answer!

 

0 件の賞賛
返信

1,663件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @JOM_alor,

The PORESET_B signal must be low till the all the supplies are stable which means there will be 0==>1 logic.

Regards,
Mrudang

0 件の賞賛
返信