Hi,
I'm testing our prototypes and I found the step-up (3V3 to 5V) I'm using to provide the USB[1,2,3]_VBUS, is quite noisy. See attached picture.
So far I have no issue on the USB links but I have not started to stress the interfaces yet.
Even if I'm inside the tolerance I would like to understand if the ac component could be an issue, and if I have to change the dcdc.
Regards
Fabio
已解决! 转到解答。