Hi,
I'm testing our prototypes and I found the step-up (3V3 to 5V) I'm using to provide the USB[1,2,3]_VBUS, is quite noisy. See attached picture.
So far I have no issue on the USB links but I have not started to stress the interfaces yet.
Even if I'm inside the tolerance I would like to understand if the ac component could be an issue, and if I have to change the dcdc.
Regards
Fabio
解決済! 解決策の投稿を見る。
Something is really wrong with the 5V converter.
Please consult with the device manufacturer support.
Something is really wrong with the 5V converter.
Please consult with the device manufacturer support.
Thanks, I'm aware of that and I'm working on that side too, therefore you're suggesting to improve it.
Have a good day