LS1021ATSN-PA PING PROBLEMS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021ATSN-PA PING PROBLEMS

2,733件の閲覧回数
972515089
Contributor II

I  am using ls1021atsn-pa board with openil,when tyied to ping PC using the command "ping ip address",it always print out the error"host unreachable". 

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,658件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please provide Linux console log and Linux Kernel booting up log.

0 件の賞賛
返信

2,658件の閲覧回数
972515089
Contributor II

Thank you for your answer,but i can not find out the log,when i connect the eth0 with consle,there is only the green light flashes, the orange one does not even lit. 

0 件の賞賛
返信

2,658件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please make sure there is no problem with the networking environment,

Please execute command arp -s <host IP address> <host HW address> on the target.

Thanks,

Yiping

0 件の賞賛
返信

2,658件の閲覧回数
972515089
Contributor II

Than you,i have solved the problem.It seems there are some problems with the command,thank you again.

0 件の賞賛
返信