LS1021ATSN-PA PING PROBLEMS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021ATSN-PA PING PROBLEMS

2,707 Views
972515089
Contributor II

I  am using ls1021atsn-pa board with openil,when tyied to ping PC using the command "ping ip address",it always print out the error"host unreachable". 

Tags (2)
0 Kudos
Reply
4 Replies

2,632 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please provide Linux console log and Linux Kernel booting up log.

0 Kudos
Reply

2,632 Views
972515089
Contributor II

Thank you for your answer,but i can not find out the log,when i connect the eth0 with consle,there is only the green light flashes, the orange one does not even lit. 

0 Kudos
Reply

2,632 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please make sure there is no problem with the networking environment,

Please execute command arp -s <host IP address> <host HW address> on the target.

Thanks,

Yiping

0 Kudos
Reply

2,632 Views
972515089
Contributor II

Than you,i have solved the problem.It seems there are some problems with the command,thank you again.

0 Kudos
Reply