LS1012A to LTE module interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A to LTE module interface

1,275件の閲覧回数
g_reshmi
Contributor II

Hi Team

 

We are planning to interface an LTE module( with USB 2.0 interface) to the LS1012A through the ULPI interface. For doing so, we are using an ULPI to USB 2.0 bridge.

Could you kindly comment on the feasibility of the solution and also if it is possible does the NXP provide drivers for ULPI as host?

Regards

タグ(1)
0 件の賞賛
返信
1 返信

1,266件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP Linux BSP supports ULPI interface on the LS1012a board. See the Section 7.2.17 in LSDK 2108 User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

 

See also part .dts file for the LS1012a in the attachment.

0 件の賞賛
返信