LS1012A to LTE module interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1012A to LTE module interface

1,281 次查看
g_reshmi
Contributor II

Hi Team

 

We are planning to interface an LTE module( with USB 2.0 interface) to the LS1012A through the ULPI interface. For doing so, we are using an ULPI to USB 2.0 bridge.

Could you kindly comment on the feasibility of the solution and also if it is possible does the NXP provide drivers for ULPI as host?

Regards

标记 (1)
0 项奖励
回复
1 回复

1,272 次查看
Pavel
NXP Employee
NXP Employee

NXP Linux BSP supports ULPI interface on the LS1012a board. See the Section 7.2.17 in LSDK 2108 User Guide:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev21.08.pdf

 

See also part .dts file for the LS1012a in the attachment.

0 项奖励
回复