LPC1763 UART DMA Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1763 UART DMA Issue

1,158件の閲覧回数
balakrishnan_ch
Contributor I

I am using LPC1763. Already verified the UART operation on my product. Now needs to use DMA for UART, especially UART0. Based on the example code provided by NXP, upated my source code. While I transmit data through UART0 by using DMA, I am not getting the expected data at the receive side of the other device. I am only receiving the value 0xFF. My message packet contains 0xFF as a first byte, maybe I am receiving only one byte data in the other side. Verified the transfer size set in the register, everything looks fine. Also to mention I am getting DMA interrupt for every Tx.

0 件の賞賛
返信
1 返信

1,116件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Balakrishnan,

If you transmit a character repeatedly for example 'A' via DMA mode, then use a scope or logic analyzer to test the TX pin of uart, you can confirm if the DMA transmitted character correctly.

You can post the code so that we can have a review.

BR

XiangJun Rong

0 件の賞賛
返信