LDMOS transistor simulation with ADS2013 - Got error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LDMOS transistor simulation with ADS2013 - Got error

3,199 Views
benyang
Contributor I

I download RF_POWER_ADS2011_DK (it's the latest version of model for MRF1518), unzipped,
added the "lib.edf" file into ADS 2013, and ran simulation, then got
an error as following:

`FSL_MRF1518NT1_MET.T1' is an instance of an undefined model
`FSLRFPK_METMOS_v1'.

can anybody pls help me to fix it? I'll appreciate it.

Ben

Labels (1)
  • RF

0 Kudos
Reply
3 Replies

2,557 Views
milanbaca
Contributor III

If you download model from our web page

Models for ADS: Agilent Advanced Design System

also you have to download RD High Power Model KIT 2012

ADS Model Kit 2012 -- simulation code to run RF High Power Model Design Kits (Required)

and it will work

0 Kudos
Reply

2,557 Views
benyang
Contributor I

Hi Milan, highly appreciate your kind help. Ben

0 Kudos
Reply

2,557 Views
benyang
Contributor I

Hi Milan, highly appreciate your kind help. Ben

0 Kudos
Reply