L4Re compile fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L4Re compile fail

Jump to solution
1,453 Views
Siyan
Contributor III

Hi, NXP Experts,

According to the description of the L4Re build environment in section ‘5.9.2.3 Build Environment‘ of the ‘UG_S32ZE_GreenVIP.pdf‘, the L4Re source code pulled via Hammer has not been modified. However, when attempting to compile the project, the following error is reported. How to solve this issue?

 

Siyan_2-1744274268719.png

 

Tags (3)
0 Kudos
Reply
1 Solution
1,392 Views
Siyan
Contributor III
Thanks, Liek. L4Re works good now.

View solution in original post

0 Kudos
Reply
2 Replies
1,406 Views
LiekLi
NXP Employee
NXP Employee

Hi Siyan,

 

Seems the SW package on github is not correct. I already send you the one which is OK on my side.

0 Kudos
Reply
1,393 Views
Siyan
Contributor III
Thanks, Liek. L4Re works good now.
0 Kudos
Reply