KITPFGUI 4.1 programming error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KITPFGUI 4.1 programming error

25,483 次查看
User_mmpf
Contributor I

I have configured the TBB tab in the GUI to my requirements. Now that I am trying to load the TBB configuration to the PMIC through programming window, I am getting these messages. Does this mean the sequencing is wrong? What is the issue here?

0 项奖励
回复
16 回复数

25,452 次查看
guoweisun
NXP TechSupport
NXP TechSupport

If you want to load the TBB script, you should operate it in the 'script editor'.

0 项奖励
回复

25,444 次查看
User_mmpf
Contributor I

Loaded it in script editor and ran it. I am trying to change the I2C address of the device to 0x0A(default 0x08). The script runs successfully. But when I am scanning the device through arduino for I2C address, it is still configured to 0x08. How do I change this?

0 项奖励
回复

25,389 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Make sure when scan operation happened,does  PMIC have power on reset? if yes,the register will recovery default.

 

0 项奖励
回复

25,384 次查看
User_mmpf
Contributor I

Only the I2C address is getting reset to default. All the other config such as voltage values, sequencing etc is as programmed in the OTP mode. Checked the power on reset as well, there is no provision for that pin in PMIC. 

0 项奖励
回复

25,382 次查看
guoweisun
NXP TechSupport
NXP TechSupport

That's indeed strange,can you share with your script here?

and execute script log?

0 项奖励
回复

25,378 次查看
User_mmpf
Contributor I

Script and run log attached

0 项奖励
回复

25,370 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Try attached script.

0 项奖励
回复

25,365 次查看
User_mmpf
Contributor I

Still reset to 0x08 after disabling and enabling supply.

0 项奖励
回复

25,363 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Do you use the new PF0100 to do OTP? If no please use new one!

0 项奖励
回复

25,361 次查看
User_mmpf
Contributor I

I have used a new one

0 项奖励
回复

25,340 次查看
User_mmpf
Contributor I

There is no functionality defined for the OTP done register. Does this need to be set after programming?

pic5 attached for reference.

0 项奖励
回复

25,441 次查看
guoweisun
NXP TechSupport
NXP TechSupport

why do you need to change the device address?

标记 (1)
0 项奖励
回复

25,439 次查看
User_mmpf
Contributor I

I am using 2 PMICs on a single board. So need two different I2C addresses. 

0 项奖励
回复

25,436 次查看
guoweisun
NXP TechSupport
NXP TechSupport

which part do you use? PF0100?

0 项奖励
回复

25,421 次查看
User_mmpf
Contributor I

YES

0 项奖励
回复

25,420 次查看
User_mmpf
Contributor I

I ran the OTP script(Programmed to 0x0A address and is working when I scan for devices: See pic1). Now after I manually powered down the PMIC i.e 3.3V supply disabled and enabled again, the address is reset to 0x08(pic2). Shouldn't the OTP config be held without supply?

0 项奖励
回复