KITPFGUI 4.1 programming error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KITPFGUI 4.1 programming error

34,989件の閲覧回数
User_mmpf
Contributor I

I have configured the TBB tab in the GUI to my requirements. Now that I am trying to load the TBB configuration to the PMIC through programming window, I am getting these messages. Does this mean the sequencing is wrong? What is the issue here?

0 件の賞賛
返信
16 返答(返信)

34,958件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If you want to load the TBB script, you should operate it in the 'script editor'.

0 件の賞賛
返信

34,946件の閲覧回数
User_mmpf
Contributor I

Loaded it in script editor and ran it. I am trying to change the I2C address of the device to 0x0A(default 0x08). The script runs successfully. But when I am scanning the device through arduino for I2C address, it is still configured to 0x08. How do I change this?

0 件の賞賛
返信

34,891件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Make sure when scan operation happened,does  PMIC have power on reset? if yes,the register will recovery default.

 

0 件の賞賛
返信

34,886件の閲覧回数
User_mmpf
Contributor I

Only the I2C address is getting reset to default. All the other config such as voltage values, sequencing etc is as programmed in the OTP mode. Checked the power on reset as well, there is no provision for that pin in PMIC. 

0 件の賞賛
返信

34,884件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

That's indeed strange,can you share with your script here?

and execute script log?

0 件の賞賛
返信

34,879件の閲覧回数
User_mmpf
Contributor I

Script and run log attached

0 件の賞賛
返信

34,871件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Try attached script.

0 件の賞賛
返信

34,866件の閲覧回数
User_mmpf
Contributor I

Still reset to 0x08 after disabling and enabling supply.

0 件の賞賛
返信

34,864件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Do you use the new PF0100 to do OTP? If no please use new one!

0 件の賞賛
返信

34,862件の閲覧回数
User_mmpf
Contributor I

I have used a new one

0 件の賞賛
返信

34,841件の閲覧回数
User_mmpf
Contributor I

There is no functionality defined for the OTP done register. Does this need to be set after programming?

pic5 attached for reference.

0 件の賞賛
返信

34,942件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

why do you need to change the device address?

タグ(1)
0 件の賞賛
返信

34,940件の閲覧回数
User_mmpf
Contributor I

I am using 2 PMICs on a single board. So need two different I2C addresses. 

0 件の賞賛
返信

34,937件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

which part do you use? PF0100?

0 件の賞賛
返信

34,922件の閲覧回数
User_mmpf
Contributor I

YES

0 件の賞賛
返信

34,920件の閲覧回数
User_mmpf
Contributor I

I ran the OTP script(Programmed to 0x0A address and is working when I scan for devices: See pic1). Now after I manually powered down the PMIC i.e 3.3V supply disabled and enabled again, the address is reset to 0x08(pic2). Shouldn't the OTP config be held without supply?

0 件の賞賛
返信