JN5189_DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5189_DMA

1,039 次查看
paidaxing
Contributor III

Hi, Teams,

We are using DMA_Init(EXAMPLE_DMA) in JN-AN-1243-Zigbee-3-0-Base-Device。

my question:

  it indicates address 0x4016060 of EndDevice/Build/mcux/EndDevice_OM15082/EndDevice_OM15082.axf section `.bss' is not within region `RAM0'.

Thanks.

0 项奖励
回复
4 回复数

973 次查看
paidaxing
Contributor III

First,I use the code in pin_mux.c of 1243 as follow:

/*s
* Copyright 2019-2020 NXP
* All rights reserved.
*
* SPDX-License-Identifier: BSD-3-Clause
*/

/***********************************************************************************************************************
* This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
* will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
**********************************************************************************************************************/

/* clang-format off */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: Pins v6.0
processor: JN5189
package_id: JN5189HN
mcu_data: ksdk2_0
processor_version: 0.0.0
pin_labels:
- {pin_num: '3', pin_signal: PIO0_0/USART0_SCK/USART1_TXD/PWM0/SPI1_SCK/PDM0_DATA, label: LED0, identifier: LED0}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
/* clang-format on */

#include "fsl_common.h"
#include "fsl_iocon.h"
#include "pin_mux.h"

/* FUNCTION ************************************************************************************************************
*
* Function Name : BOARD_InitBootPins
* Description : Calls initialization functions.
*
* END ****************************************************************************************************************/
void BOARD_InitBootPins(void)
{
BOARD_InitPins();
}

/* clang-format off */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
BOARD_InitPins:
- options: {callFromInitBoot: 'true', coreID: cm4, enableClock: 'true'}
- pin_list:
- {pin_num: '15', peripheral: SWD, signal: SWCLK, pin_signal: PIO0_12/IR_BLASTER/SWCLK/PWM0/I2C1_SCL/SPI0_MOSI/ANA_COMP_OUT, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '16', peripheral: SWD, signal: SWDIO, pin_signal: PIO0_13/SPI1_SSELN2/SWDIO/PWM2/I2C1_SDA/SPI0_SSELN, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '12', peripheral: USART0, signal: RXD, pin_signal: PIO0_9/SPI0_SSELN/USART0_RXD/CT32B1_CAP1/PWM9/USART1_SCK/ADO/PDM1_CLK, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '11', peripheral: USART0, signal: TXD, pin_signal: PIO0_8/SPI0_MOSI/USART0_TXD/CT32B0_MAT0/PWM8/ANA_COMP_OUT/RFTX/PDM1_DATA, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '19', peripheral: SPIFI, signal: CSN, pin_signal: PIO0_16/SPI1_SSELN0/ISO7816_RST/PWM5/I2C0_SDA/PDM1_CLK/SPIFI_CSN, mode: pullUp, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '22', peripheral: SPIFI, signal: SPIFI_CLK, pin_signal: PIO0_18/SPI1_MISO/ISO7816_IO/CT32B0_MAT1/PWM7/USART0_TXD/SPIFI_CLK, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '24', peripheral: SPIFI, signal: 'SPIFI_IO, 2', pin_signal: PIO0_20/IR_BLASTER/USART1_TXD/PWM8/RFTX/SPIFI_IO2, mode: pullDown, slew0: standard, invert: disabled,
filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '21', peripheral: SPIFI, signal: 'SPIFI_IO, 3', pin_signal: PIO0_17/SPI1_MOSI/ISO7816_CLK/SWO/PWM6/CLK_OUT/SPIFI_IO3, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '23', peripheral: SPIFI, signal: SPIFI_IO0_or_SPIFI_MOSI, pin_signal: PIO0_19/ADO/USART1_RXD/CLK_IN/PWM4/USART0_RXD/SPIFI_IO0, mode: pullDown, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
- {pin_num: '25', peripheral: SPIFI, signal: SPIFI_IO1_or_SPIFI_MISO, pin_signal: PIO0_21/IR_BLASTER/USART1_SCK/PWM9/RFRX/SWO/SPIFI_IO1, mode: pullUp, slew0: standard,
invert: disabled, filter_off: disabled, slew1: standard, open_drain: disabled, ssel: disabled}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
/* clang-format on */

/* FUNCTION ************************************************************************************************************
*
* Function Name : BOARD_InitPins
* Description : Configures pin routing and optionally pin electrical features.
*
* END ****************************************************************************************************************/
/* Function assigned for the Cortex-M4 */
void BOARD_InitPins(void)
{
/* Enables the clock for the I/O controller block. 0: Disable. 1: Enable.: 0x01u */
CLOCK_EnableClock(kCLOCK_Iocon);

const uint32_t port0_pin12_config = (/* Pin is configured as SWCLK */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN12 (coords: 15) is configured as SWCLK */
IOCON_PinMuxSet(IOCON, 0U, 12U, port0_pin12_config);

const uint32_t port0_pin13_config = (/* Pin is configured as SWDIO */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN13 (coords: 16) is configured as SWDIO */
IOCON_PinMuxSet(IOCON, 0U, 13U, port0_pin13_config);

const uint32_t port0_pin16_config = (/* Pin is configured as SPIFI_CSN */
IOCON_PIO_FUNC7 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN16 (coords: 19) is configured as SPIFI_CSN */
IOCON_PinMuxSet(IOCON, 0U, 16U, port0_pin16_config);

const uint32_t port0_pin17_config = (/* Pin is configured as SPIFI_IO3 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN17 (coords: 21) is configured as SPIFI_IO3 */
IOCON_PinMuxSet(IOCON, 0U, 17U, port0_pin17_config);

const uint32_t port0_pin18_config = (/* Pin is configured as SPIFI_CLK */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN18 (coords: 22) is configured as SPIFI_CLK */
IOCON_PinMuxSet(IOCON, 0U, 18U, port0_pin18_config);

const uint32_t port0_pin19_config = (/* Pin is configured as SPIFI_IO0 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN19 (coords: 23) is configured as SPIFI_IO0 */
IOCON_PinMuxSet(IOCON, 0U, 19U, port0_pin19_config);

const uint32_t port0_pin20_config = (/* Pin is configured as SPIFI_IO2 */
IOCON_PIO_FUNC7 |
/* Selects pull-down function */
IOCON_PIO_MODE_PULLDOWN |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN20 (coords: 24) is configured as SPIFI_IO2 */
IOCON_PinMuxSet(IOCON, 0U, 20U, port0_pin20_config);

const uint32_t port0_pin21_config = (/* Pin is configured as SPIFI_IO1 */
IOCON_PIO_FUNC7 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN21 (coords: 25) is configured as SPIFI_IO1 */
IOCON_PinMuxSet(IOCON, 0U, 21U, port0_pin21_config);

const uint32_t port0_pin8_config = (/* Pin is configured as USART0_TXD */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN8 (coords: 11) is configured as USART0_TXD */
IOCON_PinMuxSet(IOCON, 0U, 8U, port0_pin8_config);

const uint32_t port0_pin9_config = (/* Pin is configured as USART0_RXD */
IOCON_PIO_FUNC2 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW0_STANDARD |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is disabled */
IOCON_PIO_SLEW1_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI |
/* SSEL is disabled */
IOCON_PIO_SSEL_DI);
/* PORT0 PIN9 (coords: 12) is configured as USART0_RXD */
IOCON_PinMuxSet(IOCON, 0U, 9U, port0_pin9_config);
}
/***********************************************************************************************************************
* EOF
**********************************************************************************************************************/

second,i create a source flie in EndDevice to realize my DMA,the code are as follow:

#define CLOCK_ABSTRACTION
/* Abstract attaching the clock */
#define EXAMPLE_SPIFI_CLK_SRC (kMAIN_CLK_to_SPIFI)
#define EXAMPLE_SPIFI_ATTACH_MAIN_CLK (CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC))
/* Abstract getting the clock */
#define EXAMPLE_SPIFI_CLK (kCLOCK_Spifi)
#define EXAMPLE_SPIFI_CLOCK_FREQ (CLOCK_GetFreq(EXAMPLE_SPIFI_CLK))

#define EXAMPLE_DMA (DMA0)
#define EXAMPLE_SPIFI_CHANNEL (12)

#define EXAMPLE_SPIFI SPIFI
#define PAGE_SIZE (256)
#define SECTOR_SIZE (4096)
#define EXAMPLE_SPI_BAUDRATE (16000000L)
static spifi_dma_handle_t handle;
static dma_handle_t s_DmaHandle;
typedef enum _command_t
{
// RDID, /* Write Status Register */
// RDSR, /* Read Status Register */
// RDCR, /* Read Configuration Register */
// WREN, /* Write Enable */
// WRDI, /* Write Disable */
// WRSR, /* Write Status Register */
// PP4, /* Quad Page Program */
// QPP, /* Quad Input Page Program */
// QREAD, /* 1I-4O read */
// SE, /* Sector Erase */
//READ, /* Read */
//DREAD, /* 1I-2O read */
// READ2, /* 2I-2O read */
// PP, /* Page Program */
// READ4, /* 4I-4O read */
//BE64K, /* Block Erase */
//BE32K, /* Block Erase */
// CE, /* Chip Erase */
// DP, /* Deep Power Down */
RSTEN, /* Reset Enable*/
RST, /* Reset*/
MAX_CMD
} command_t;
/*******************************************************************************
* Variables
******************************************************************************/
spifi_command_t command[] = {
// [RDID] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x9F},
//[RDSR] = {1, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x05},
//[RDCR] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x15},
//[WREN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x06},
//[WRDI] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x04},
//[WRSR] = {3, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x01},
//[PP4] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes,0x38},
//[QPP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x32},
//[QREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x6B},
//[SE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x20},
//[READ] = {PAGE_SIZE, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x03},
//[DREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x3B},
//[READ2] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xBB},
// [PP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x02},
// [READ4] = {PAGE_SIZE, false, kSPIFI_DataInput, 3, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xEB},
// [BE64K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xD8},
//[BE32K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x52},
//[CE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x60},
//[DP] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0xB9},
[RSTEN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x66},
[RST] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x99},
};
static volatile bool finished = false;
PUBLIC void callback(SPIFI_Type *base, spifi_dma_handle_t *handle, status_t status, void *userData)
{
finished = true;
}
PUBLIC void flash()
{ spifi_config_t config = {0};
/* Init the boards */
/* Security code to allow debug access */
SYSCON->CODESECURITYPROT = 0x87654320;

/* attach clock for USART(debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

/* reset FLEXCOMM for USART */
RESET_PeripheralReset(kFC0_RST_SHIFT_RSTn);
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
BOARD_InitPins();
uint32_t sourceClockFreq;

/* Set SPIFI clock source */
CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC);
sourceClockFreq = CLOCK_GetSpifiClkFreq();
/* Set the clock divider */
uint32_t divisor;
/* Do not set null divisor value */
divisor = sourceClockFreq / EXAMPLE_SPI_BAUDRATE;
CLOCK_SetClkDiv(kCLOCK_DivSpifiClk, divisor ? divisor : 1, false);
PRINTF("SPIFI flash dma example started \r\n");
//开始
DMA_Init(EXAMPLE_DMA);

DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
DMA_CreateHandle(&s_DmaHandle, EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12

/* Initialize SPIFI */
SPIFI_GetDefaultConfig(&config);
SPIFI_Init(EXAMPLE_SPIFI, &config);
/* Reset the SPIFI to switch to command mode */
SPIFI_ResetCommand(EXAMPLE_SPIFI);
SPIFI_TransferRxCreateHandleDMA(EXAMPLE_SPIFI, &handle, callback, NULL, &s_DmaHandle);

/* Reset Device*/
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RSTEN]);//重置使能
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RST]);//重置SPI

}

#define CLOCK_ABSTRACTION
/* Abstract attaching the clock */
#define EXAMPLE_SPIFI_CLK_SRC (kMAIN_CLK_to_SPIFI)
#define EXAMPLE_SPIFI_ATTACH_MAIN_CLK (CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC))
/* Abstract getting the clock */
#define EXAMPLE_SPIFI_CLK (kCLOCK_Spifi)
#define EXAMPLE_SPIFI_CLOCK_FREQ (CLOCK_GetFreq(EXAMPLE_SPIFI_CLK))

#define EXAMPLE_DMA (DMA0)
#define EXAMPLE_SPIFI_CHANNEL (12)

#define EXAMPLE_SPIFI SPIFI
#define PAGE_SIZE (256)
#define SECTOR_SIZE (4096)
#define EXAMPLE_SPI_BAUDRATE (16000000L)
static spifi_dma_handle_t handle;
static dma_handle_t s_DmaHandle;
typedef enum _command_t
{
// RDID, /* Write Status Register */
// RDSR, /* Read Status Register */
// RDCR, /* Read Configuration Register */
// WREN, /* Write Enable */
// WRDI, /* Write Disable */
// WRSR, /* Write Status Register */
// PP4, /* Quad Page Program */
// QPP, /* Quad Input Page Program */
// QREAD, /* 1I-4O read */
// SE, /* Sector Erase */
//READ, /* Read */
//DREAD, /* 1I-2O read */
// READ2, /* 2I-2O read */
// PP, /* Page Program */
// READ4, /* 4I-4O read */
//BE64K, /* Block Erase */
//BE32K, /* Block Erase */
// CE, /* Chip Erase */
// DP, /* Deep Power Down */
RSTEN, /* Reset Enable*/
RST, /* Reset*/
MAX_CMD
} command_t;
/*******************************************************************************
* Variables
******************************************************************************/
spifi_command_t command[] = {
// [RDID] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x9F},
//[RDSR] = {1, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x05},
//[RDCR] = {4, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x15},
//[WREN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x06},
//[WRDI] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x04},
//[WRSR] = {3, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x01},
//[PP4] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes,0x38},
//[QPP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x32},
//[QREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x6B},
//[SE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x20},
//[READ] = {PAGE_SIZE, false, kSPIFI_DataInput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x03},
//[DREAD] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandDataQuad, kSPIFI_CommandOpcodeAddrThreeBytes, 0x3B},
//[READ2] = {PAGE_SIZE, false, kSPIFI_DataInput, 1, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xBB},
// [PP] = {PAGE_SIZE, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x02},
// [READ4] = {PAGE_SIZE, false, kSPIFI_DataInput, 3, kSPIFI_CommandOpcodeSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xEB},
// [BE64K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0xD8},
//[BE32K] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeAddrThreeBytes, 0x52},
//[CE] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x60},
//[DP] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0xB9},
[RSTEN] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x66},
[RST] = {0, false, kSPIFI_DataOutput, 0, kSPIFI_CommandAllSerial, kSPIFI_CommandOpcodeOnly, 0x99},
};
static volatile bool finished = false;
PUBLIC void callback(SPIFI_Type *base, spifi_dma_handle_t *handle, status_t status, void *userData)
{
finished = true;
}
PUBLIC void flash()
{ spifi_config_t config = {0};
/* Init the boards */
/* Security code to allow debug access */
SYSCON->CODESECURITYPROT = 0x87654320;

/* attach clock for USART(debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

/* reset FLEXCOMM for USART */
RESET_PeripheralReset(kFC0_RST_SHIFT_RSTn);
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
BOARD_InitPins();
uint32_t sourceClockFreq;

/* Set SPIFI clock source */
CLOCK_AttachClk(EXAMPLE_SPIFI_CLK_SRC);
sourceClockFreq = CLOCK_GetSpifiClkFreq();
/* Set the clock divider */
uint32_t divisor;
/* Do not set null divisor value */
divisor = sourceClockFreq / EXAMPLE_SPI_BAUDRATE;
CLOCK_SetClkDiv(kCLOCK_DivSpifiClk, divisor ? divisor : 1, false);
PRINTF("SPIFI flash dma example started \r\n");
//开始
DMA_Init(EXAMPLE_DMA);

DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12
DMA_CreateHandle(&s_DmaHandle, EXAMPLE_DMA, EXAMPLE_SPIFI_CHANNEL);//通道12

/* Initialize SPIFI */
SPIFI_GetDefaultConfig(&config);
SPIFI_Init(EXAMPLE_SPIFI, &config);
/* Reset the SPIFI to switch to command mode */
SPIFI_ResetCommand(EXAMPLE_SPIFI);
SPIFI_TransferRxCreateHandleDMA(EXAMPLE_SPIFI, &handle, callback, NULL, &s_DmaHandle);

/* Reset Device*/
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RSTEN]);//重置使能
SPIFI_SetCommand(EXAMPLE_SPIFI, &command[RST]);//重置SPI

}

My question :When i call the function flash i created , 

it indicates address 0x4016060 of EndDevice/Build/mcux/EndDevice_OM15082/EndDevice_OM15082.axf section `.bss' is not within region `RAM0'.

Thanks.

0 项奖励
回复

1,022 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please give us more details about your question? Did you modify the JN-AN-1243? What AN version are you using? (You can find the version on the Version.txt file) What SDK version are you using?

 

Regards,

Ricardo

0 项奖励
回复

999 次查看
paidaxing
Contributor III

Thank you for your reply .I modify the pin_mux.c and pin_mux.h of 1243.The version of AN is 2006.SDK version is 2.6.5(2022-3-10).

0 项奖励
回复

977 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Thank you, but could you please let us know the modifications you made?

And also, could you clarify your original question?

 

Regards,

Ricardo

0 项奖励
回复