Issue reading registers in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue reading registers in u-boot

跳至解决方案
4,096 次查看
Ghouse
Contributor V

Hi, iam using LS1046ARDB eval board,

An iam working on secure boot,

The procudure to secure boot says : "Verify the SNVS register - HPSR to check whether OTPMK is fused already" by using command md $SNVS_HPSR_REG,

however when i execute above command in u boot iam getting below message

md - memory display

Usage:
md [.b, .w, .l, .q] address [# of objects]

but, when i read register w.r.t address (eg: md 0x01e80254 0x10) iam able to read it.

Let me know the exact syntax to read the register by providing register name in the u-boot console.

Thanks.

 

0 项奖励
回复
1 解答
4,042 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please use the following command.

=> md 0x1e90014

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,093 次查看
John_volvo
Contributor I

if OTPMK is fused already, whether can use reset to default value? or need replace chip? 

0 项奖励
回复
4,048 次查看
Ghouse
Contributor V

Hi, any help for the above query?

Thanks.

0 项奖励
回复
4,043 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please use the following command.

=> md 0x1e90014

0 项奖励
回复
3,930 次查看
tdemke
Contributor I

On my LS1046ardb board:

=> md 0x1e90014
01e90014: 002b0088 00000080 00000000 00000000    ..+.............

This is not inline with the documentation!

=> md $SNVS_HPSR_REG
88000900

So how can we check in u-boot if the OTPMK values are written?

0 项奖励
回复