Is TDF8546ATH/N1ZJ replaceable with TDF8546TH/N2Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is TDF8546ATH/N1ZJ replaceable with TDF8546TH/N2Z?

Jump to solution
2,506 Views
Bobbobbob
Contributor II

Hi, this is Bob.

 

I would like to know if TDF8546ATH/N1ZJ is replaceable with TDF8546TH/N2Z.

is it okay to apply TDF8546ATH/N1ZJ? 

according to the datasheet, it says redesign. Please help confirm.

 

original usage : TDF8546TH/N2Z

NEW SUGGESTION : TDF8546ATH/N1ZJ

 

+ Can I know what is N1 / N2 / Z meaning?

I think Z / J means T&R. can you check is this right?

 

thank you so much in advance.

Best regards,

0 Kudos
Reply
1 Solution
2,496 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Bob,

https://www.nxp.com/part/TDF8546TH#/

J means plastic DIL-bent-SIL (special bent) power package; 27 leads (lead length 6.8 mm) = SOT827-1

N1Z or N2Z is the fab differentiator

https://www.nxp.com/products/power-management/wireless-power/one-chip-5-v-qi-wireless-transmitter:NX...

The TDF8546A is a redesign of the TDF8546 having a lower quiescent current and improved electromagnetic immunity (EMI) properties. The TDF8546 and TDF8546A use an asymmetrical input configuration, delivers 25 W of output power, and is available in several bend variants of DBS27 or HSOP36 package.

Please refer to: https://www.nxp.com/docs/en/brochure/75017414.pdf

Best regards

Pavla

View solution in original post

0 Kudos
Reply
2 Replies
2,497 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Bob,

https://www.nxp.com/part/TDF8546TH#/

J means plastic DIL-bent-SIL (special bent) power package; 27 leads (lead length 6.8 mm) = SOT827-1

N1Z or N2Z is the fab differentiator

https://www.nxp.com/products/power-management/wireless-power/one-chip-5-v-qi-wireless-transmitter:NX...

The TDF8546A is a redesign of the TDF8546 having a lower quiescent current and improved electromagnetic immunity (EMI) properties. The TDF8546 and TDF8546A use an asymmetrical input configuration, delivers 25 W of output power, and is available in several bend variants of DBS27 or HSOP36 package.

Please refer to: https://www.nxp.com/docs/en/brochure/75017414.pdf

Best regards

Pavla

0 Kudos
Reply
2,465 Views
Bobbobbob
Contributor II

Dear Pavla,

 

thank you for the kind reply.

can you also check what is Z stands for?

TDF8546TH/N2Z

0 Kudos
Reply