Interfacing MC33771B with Arduino UNO using SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing MC33771B with Arduino UNO using SPI

Jump to solution
11,279 Views
ashutosh_saxena
Contributor I

I want help with interfacing MC33771B with Arduino UNO using SPI communication. I am trying to receive the cell values of my battery pack, but I am unable to do so. Can anyone help me with example codes or if someone has already worked on the same, can you please share the code.

0 Kudos
Reply
1 Solution
11,213 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below picture showed code, this GUI design based on KL25Z.

guoweisun_0-1668066910266.png

 

View solution in original post

0 Kudos
Reply
14 Replies
11,258 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can sign NDA then download it in the NXP website.

Search | NXP Semiconductors

guoweisun_0-1667980727346.png

 

0 Kudos
Reply
11,258 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
11,253 Views
ashutosh_saxena
Contributor I

We have already downloaded BCC driver software and it is not helping us to establish SPI communication/ fetch data.

0 Kudos
Reply
11,256 Views
ashutosh_saxena
Contributor I

Our company has signed NDA with NXP earlier. 

0 Kudos
Reply
11,252 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to directly download it!

0 Kudos
Reply
11,218 Views
ashutosh_saxena
Contributor I

It shows Arduino as an option in Eval GUI, but it is not selectable. How can I solve this?

0 Kudos
Reply
11,216 Views
guoweisun
NXP TechSupport
NXP TechSupport

 

guoweisun_0-1668065400366.png

You can try to re-set the jumper in the FRDM33771BSPIEVB.

 

0 Kudos
Reply
11,214 Views
ashutosh_saxena
Contributor I

Tried that multiple times, but it is not acknowledging Arduino even after updating the port in device manager. 

0 Kudos
Reply
11,214 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below picture showed code, this GUI design based on KL25Z.

guoweisun_0-1668066910266.png

 

0 Kudos
Reply
11,212 Views
guoweisun
NXP TechSupport
NXP TechSupport

What's your control board? KL25Z? S32?

 

0 Kudos
Reply
11,210 Views
ashutosh_saxena
Contributor I

As of now I am using Arduino as control board and MC33771B as AFE (Cell controller).

0 Kudos
Reply
11,240 Views
ashutosh_saxena
Contributor I

The examples given in the BCC driver folder are for NXP MCU and NXP AFE. I want to configure NXP AFE (MC33771B)  with Arduino UNO.

0 Kudos
Reply
9,049 Views
Shobha
Contributor I

Hey I want to interface MC33771(BCC) with Arduino. Could you pl help me with this if you got the solution for your doubts mentioned here.

0 Kudos
Reply
11,228 Views
ashutosh_saxena
Contributor I

If I have S32K144 evaluation board, will I be able to establish SPI successfully? Is it the same programming that is available in S32 DS ARM IDE.

0 Kudos
Reply