Implementing Positioning Algorithms Using Accelerometers AN3397

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing Positioning Algorithms Using Accelerometers AN3397

2,735 Views
yellingdog
Contributor I

Hi,

I'm reading the application note AN3397 and was wondering in what unit is the measured position in?

In the note I don't see Time being a variable anywhere. It is stated that the time between samples MUST be the same however.

So a is in m/s2

v is in m/s ?

and positionX in what?

Here are the integrations I'm doing, with sampling rate 1.5ms:

velocityx[1]= velocityx[0]+ accelerationx[0]+ ((accelerationx[1] -accelerationx[0])/2)*0.0015;
positionX[1]= positionX[0] + velocityx[0] + ((velocityx[1] - velocityx[0])/2)*0.0015;

Do they seem correct?

thanks

Tags (3)
0 Kudos
Reply
3 Replies

2,701 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

You are correct, in this case the time between samples MUST always be the same. Errors can be generated if this time is not equal. I do recommend a faster sampling frequency for accurate results.

So a double integration of your samples (after a double filtering process and calibration) is the requirement needed to obtain the position using the acceleration data.

 

I hope this information helps.

Regards,

David

0 Kudos
Reply

2,722 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

The position is expressed in m (meters).

Note that in order to create a coherent value, sampling time must always be the same.

 

I hope this information helps.

Regards,

David

0 Kudos
Reply

2,717 Views
yellingdog
Contributor I

Hi David,

So T doesn't have to be included in the calculations as long as it is a constant?

thanks

0 Kudos
Reply