IO communication interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IO communication interface

ソリューションへジャンプ
1,480件の閲覧回数
buku
Contributor I

I have a display (NHD-C12864KGZ-FSW-GBW) which has D0-D7 bidirectional data line pins, So Can i connect this device pins directly to pins of PCAL6524HEAZ?

Kind Regards,

Kunal

0 件の賞賛
返信
1 解決策
1,468件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Kunal,

yes, you can connect D0-D7 bidirectional data pins directly to the directly to pins of PCAL6524HEAZ. Please make sure the voltage levels of PCAL6524 are set for the voltage levels of the NHD-C12864KGZ-FSW-GBW.

JozefKozon_1-1624341162342.pngJozefKozon_1-1624341162342.png

JozefKozon_0-1624341147780.pngJozefKozon_0-1624341147780.png

With Best Regards,

Jozef

 

元の投稿で解決策を見る

1 返信
1,469件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Kunal,

yes, you can connect D0-D7 bidirectional data pins directly to the directly to pins of PCAL6524HEAZ. Please make sure the voltage levels of PCAL6524 are set for the voltage levels of the NHD-C12864KGZ-FSW-GBW.

JozefKozon_1-1624341162342.pngJozefKozon_1-1624341162342.png

JozefKozon_0-1624341147780.pngJozefKozon_0-1624341147780.png

With Best Regards,

Jozef