IMX8mp with Atmel Touch Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8mp with Atmel Touch Interface

1,558 次查看
Aditya2125
Contributor I

Hello,

I am using imx8mp custom board and i have interfaced atmel touch with custom board.

below is device tree configuration:

&i2c5 {
clock-frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c5>;
status = "okay";

touchscreen@4b {
compatible = "atmel,maxtouch";
reg = <0x4b>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_touch_p1>;
interrupt-parent = <&gpio2>;
interrupts = <4 IRQ_TYPE_EDGE_FALLING>;
reset-gpios = <&gpio2 5 GPIO_ACTIVE_LOW>;
status = "okay";
};
};

pinctrl_i2c5: i2c5grp {
fsl,pins = <
MX8MP_IOMUXC_SD1_CLK__I2C5_SCL 0x400001c2
MX8MP_IOMUXC_SD1_CMD__I2C5_SDA 0x400001c2
>;
};


pinctrl_touch_p1: touchgrp {
fsl,pins = <
MX8MP_IOMUXC_SD1_DATA2__GPIO2_IO04 0x16 /* TS_CHG */
MX8MP_IOMUXC_SD1_DATA3__GPIO2_IO05 0x16 /* TS_RST */
>;
};


Debug UART log

[ 2.223601][ T1] atmel_mxt_ts 4-004b: __mxt_read_reg: i2c transfer failed (-6)
[ 2.231710][ T1] atmel_mxt_ts 4-004b: mxt_bootloader_read: i2c recv failed (-6)
[ 2.239300][ T1] atmel_mxt_ts 4-004b: Trying alternate bootloader address
[ 2.247182][ T1] atmel_mxt_ts 4-004b: mxt_bootloader_read: i2c recv failed (-6)


Below are the i2c lines voltages:
I2C_SCL -> 3.19v (Pull-up 4.7k Resistor included)
I2C_SDA -> 3.13v (Pull-up 4.7k Resistor included)

After this configuration touch is not working, Please suggest suitable solution.

Thanks,

 

0 项奖励
回复
1 回复

1,531 次查看
Aditya2125
Contributor I

we have tested also this: but results and logs are same.

pinctrl_i2c5: i2c5grp {
fsl,pins = <
MX8MP_IOMUXC_SD1_CLK__I2C5_SCL 0x400001c3
MX8MP_IOMUXC_SD1_CMD__I2C5_SDA 0x400001c3
>;
};

0 项奖励
回复