IC marking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IC marking

2,854 Views
logivoid
Contributor I

Hi, does anyone know this IC?


Marking:

282 11 910

F2Y1261

EnD1538

Also, on board placed ic's (282 11 894), (282 11 882).

Most of them are water-damaged.
I assume this is some kind of load drivers, but can't find any data

photo1660645075.jpgphoto1660645075.jpg

0 Kudos
Reply
1 Reply

2,848 Views
JaniMar
NXP TechSupport
NXP TechSupport

Thank you for your inquiry.

Based on the top marking shared, this part was recognized as a valid part however it is marked as Customer Specific.
It means that this device was made by NXP based on specific contract for the specific company, only they can obtain the information, all information is confidential.

Our support center is not authorized to check or release information as we do not have an access. We can provide support for standard parts only.

The company for whom this device was made needs to contact their representative inside NXP who can provide more info.

If the MCUs are part of the board in your car, you may need to contact the producer of the component where NXP part was implemented.

Thank you for your understanding.

0 Kudos
Reply