How to install packages on i.mx 8 BSP Linux OS using apt-get ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to install packages on i.mx 8 BSP Linux OS using apt-get ?

2,288件の閲覧回数
bckpoojary
Contributor I

Hi,

I'm trying to install few packages on Linux  6.1.36 OS installed i.mx 8 nano board using apt-get install command, but for each packages I'm getting an error message like 'Unable to locate package <package name>. can you please help on this how to get resolve this issue. attachment I have uploaded below.

Thank you

 

0 件の賞賛
返信
3 返答(返信)

2,250件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

 

I suggest you take a look on next post.

 

Best regards.

0 件の賞賛
返信

2,230件の閲覧回数
bckpoojary
Contributor I

Hi @JorgeCas , thank you for your response.

Here i'm not using Yocto project or any other tool to create image, I just downloaded default BSP image zip file from NXP portal and flashed into emmc. can't we add packages into default  BSP Linux OS ?

Best Regards

 

0 件の賞賛
返信

2,213件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

The i.MX BSP does not have a package manager like apt-get. You would need to add it to the Linux image. There is some information on the following documents, although further customization would be required.

 

https://community.nxp.com/docs/DOC-328199

 

https://community.nxp.com/message/834043?commentID=834043#comment-834043

 

Also, you could try to use NXP Linux Yocto Project BSP for Desktop PoC (it has package manager).

 

Best regards.

0 件の賞賛
返信