Hello NXP Community,
I am a beginner in the field of AI/ML and currently working on deploying a machine learning model on the i.MX93 evaluation board.
I have connected the i.MX93 board using two USB Type-C cables – one to the power port and the other to the debug port. Additionally, an HDMI cable is connected to a monitor to display the output. The board is powered on and appears to be functioning normally.
However, the device is not appearing in the "Remote Device" list on the development environment. I am unsure why the board is not being detected and would appreciate any guidance regarding this issue.
Could someone please help me understand:
Why the i.MX93 might not be showing up as a remote device?
How to troubleshoot this detection issue?
What should be the next steps to successfully deploy an AI/ML model on the i.MX93 board?
Any assistance or suggestions would be greatly appreciated.