How to configure GPIO as output port for MPC5604B(32 bit)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure GPIO as output port for MPC5604B(32 bit)

ソリューションへジャンプ
2,184件の閲覧回数
shri
Contributor II

i'am new to this MPC5604B 32 bit controller.i wanted to make port F as output port.how do i make it. And i need to send 16bit data out of these port continuosly .how do i do it.Will this piece of code work.Thank you.

 

for(j=0;j<16;j++)

{

SIU.PCR[80 + j].R = 0x0200;

}

while(1)

{

SIU.PGPDO[2].R = 0x0000FFFF;

}

 

タグ(2)
0 件の賞賛
返信
1 解決策
1,574件の閲覧回数
shri
Contributor II

Oh my god, I got it

instead of 

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0200;

}

i did used this

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0203;

}

Now it works

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,574件の閲覧回数
shri
Contributor II

why no one replying to this question.it is very urgent.plz replay

0 件の賞賛
返信
1,574件の閲覧回数
TomE
Specialist II

> why no one replying to this question.it is very urgent.plz replay

 

Mainly because your code doesn't show the sending of any data at all. You don't say what sort of output you want. Do you want to control single bits on and off or are you trying to write data to a 16 bit peripheral? If you want the latter then tou haven't mentioned write strobes or control pins.

 

if it is so urgent, have you TRIED your code at all? What happened?

 

Have you searched for example code anywhere? Have you downloaded Linux ports and looked for examples?

 

for(j=0;j<16;j++){    SIU.PCR[80 + j].R = 0x0200;}

 That looks like it should set the 16 pins to be GPIO outputs.

 

while(1){    SIU.PGPDO[2].R = 0x0000FFFF;}

 Without seeing the code that defines what ".R" means I have no idea. You want to write your user data as a 16-bit write to the lower 16 bits. There's probably a definition in the header where ".R" means 32-bit write and there are two other ones that mean "16 bit upper" and "16 bit lower". You should be using one of them.

 

Continuously writing in a hard loop isn't going to do anything useful. You only have to write data ONCE for the port to then drive that data until you write something else to the port.


Tom

 

0 件の賞賛
返信
1,575件の閲覧回数
shri
Contributor II

Oh my god, I got it

instead of 

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0200;

}

i did used this

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0203;

}

Now it works

 

 

0 件の賞賛
返信