How to configure GPIO as output port for MPC5604B(32 bit)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure GPIO as output port for MPC5604B(32 bit)

跳至解决方案
2,172 次查看
shri
Contributor II

i'am new to this MPC5604B 32 bit controller.i wanted to make port F as output port.how do i make it. And i need to send 16bit data out of these port continuosly .how do i do it.Will this piece of code work.Thank you.

 

for(j=0;j<16;j++)

{

SIU.PCR[80 + j].R = 0x0200;

}

while(1)

{

SIU.PGPDO[2].R = 0x0000FFFF;

}

 

标记 (2)
0 项奖励
回复
1 解答
1,562 次查看
shri
Contributor II

Oh my god, I got it

instead of 

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0200;

}

i did used this

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0203;

}

Now it works

 

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,562 次查看
shri
Contributor II

why no one replying to this question.it is very urgent.plz replay

0 项奖励
回复
1,562 次查看
TomE
Specialist II

> why no one replying to this question.it is very urgent.plz replay

 

Mainly because your code doesn't show the sending of any data at all. You don't say what sort of output you want. Do you want to control single bits on and off or are you trying to write data to a 16 bit peripheral? If you want the latter then tou haven't mentioned write strobes or control pins.

 

if it is so urgent, have you TRIED your code at all? What happened?

 

Have you searched for example code anywhere? Have you downloaded Linux ports and looked for examples?

 

for(j=0;j<16;j++){    SIU.PCR[80 + j].R = 0x0200;}

 That looks like it should set the 16 pins to be GPIO outputs.

 

while(1){    SIU.PGPDO[2].R = 0x0000FFFF;}

 Without seeing the code that defines what ".R" means I have no idea. You want to write your user data as a 16-bit write to the lower 16 bits. There's probably a definition in the header where ".R" means 32-bit write and there are two other ones that mean "16 bit upper" and "16 bit lower". You should be using one of them.

 

Continuously writing in a hard loop isn't going to do anything useful. You only have to write data ONCE for the port to then drive that data until you write something else to the port.


Tom

 

0 项奖励
回复
1,563 次查看
shri
Contributor II

Oh my god, I got it

instead of 

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0200;

}

i did used this

for(j=0;j<16;j++)

{

 SIU.PCR.R[80+j] = 0x0203;

}

Now it works

 

 

0 项奖励
回复