How to Enable DMA for USB for IMX8M Plus based on Linux kernel 6.6.54

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable DMA for USB for IMX8M Plus based on Linux kernel 6.6.54

2,307件の閲覧回数
radhak4x
Contributor II

Hi 

 

I am trying to enable DMA for USB based on linux kernel 6.6.54. what are the required changes that are needed as part of dtb's along with driver changes? 

also what is the maximum hardware buffer that is used in transfer by default for 2.0 and 3.0

 

appreciate your support here 

i am referring to ehci-hcd.c - drivers/usb/host/ehci-hcd.c - Linux source code v6.6.54 - Bootlin Elixir Cross Referenc... source code

DTB changes as per my understanding:

&usb1 {
status = "okay";
dr_mode = "host";
dma-coherent;
#address-cells = <1>;
#size-cells = <0>;
};

is this correct ? what are the driver changes needed  to enable DMA for USB 

0 件の賞賛
返信
5 返答(返信)

2,272件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

It has an embedded DMA controller in each core. DMA doesn't need to be enabled and you can reference your nodes in EVK nodes.

For TX, the USB DMA source is system memory and the destination is the USB module internal FIFO. For RX, the source is the USB controller FIFO and destination is system memory.

The DMA is used to transfer the data between Tx/RxBuffer and the controller in summary and there you can also find the DMA range.

Doc for DWC3.

Regards

0 件の賞賛
返信

2,206件の閲覧回数
radhak4x
Contributor II

Hi Joseph,

Could you please elaborate what is meant by EVK nodes?

In reference manual, could you please point - where that USB already has Embedded DMA in it.

as we don't see / not found that part in IMX8 Ref Manual?

0 件の賞賛
返信

2,132件の閲覧回数
radhak4x
Contributor II
Hi joseph,

Could you please elaborate the same ?

thanks
Radha
0 件の賞賛
返信

2,108件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi @radhak4x,

I'm still researching this issue, I will clarify it, thank you for your patience.

Regards,

0 件の賞賛
返信

2,305件の閲覧回数
radhak4x
Contributor II

What is the maximum hardware buffer defined for this ? i have referred to Reference manual - i.MX 8M Plus Applications Processor Reference Manual chapter 11 and i hardly found this data.

0 件の賞賛
返信