Hi,everybody,i'm using DSC MC56F8366 and developing Bootloader for it.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,everybody,i'm using DSC MC56F8366 and developing Bootloader for it.

1,687 Views
wzqwzq
Contributor I

I download my applitions with SCI.But i only can download with 9600 bps.When I use 19200,56000,115200.....,MCU always return an error.Can you help me?

0 Kudos
Reply
2 Replies

1,594 Views
Ben
Senior Contributor I

Hi XianJun, I have an active developments with the NC56F8367 and the 56F8257. I did not activate the bootloader yet, but I don't understand:

Did you have a  problem with freescale bootloader application? why did you have to develop your own SW?

Sorry that I can't answer your question yet, but I'll be glad to get any tip for me for the bootloader  issue, as I'll have to add bootloader.

Thanks

Benny

0 Kudos
Reply

1,594 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

sorry for the delay, I see your question just now. I do not know if you have solved your problem or not yet.

If you want to use the other baud rate, the baud rate in the bootloader code and the HyperTerminal setting should matches, I suppose you download code via Hyperterminal tools.

BR

XiangJun Rong