HVBMS Example Source Code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HVBMS Example Source Code

1,104件の閲覧回数
ArushThomas
Contributor III

Hi all,

We are interested in purchasing one of the HVBMS Bundles in order to develop software for HVBMS applications. I'm hoping to find some example source code to bringup the bundle, and use as a base to develop our application firmware.

I was able to find NXP's Automotive Software Package Manager, but got stuck in downloading the packages. I get the "this use case is disabled because it contains only disabled packages" error, seemingly on every single package.

ContainsDisabledPackages.jpg

How do I acquire example source code for these bundles?

0 件の賞賛
返信
1 返信

1,083件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ArushThomas 

You can find the S32K3 HVBMS Software Package on the main Battery Management Systems (BMS) page, under the Software section. This will redirect you to the*Automotive Software Package, where several examples and projects are available, some of which you might already be familiar with.

Please note that some of these examples are under access control and also part of the Premium package, which may require a fee. If you already have access, I recommend reaching out to one of our authorized distributors (Distributor Network) closest to your location to request access to the Premium content. Just keep in mind that this material is shared under NDA.

Also, there is a discussion on this topic in the following thread that might be helpful.

HVBMS_StartUp_FreeMASTER.elf

 

BR, VaneB

0 件の賞賛
返信