GD3160 HB-EVBs & Customized code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GD3160 HB-EVBs & Customized code

4,463件の閲覧回数
AbdulHaleemMalik
Contributor I

Hello!

I have the GD3160 Half bridge EVBs and seek your guidance if its possible to generate burst of pulses (Square wave) on the GL & HL pins (on EVBs board) at certain constant interval and rest of the time should be kept at low level. 

Please advise if its possible to get it done using Flex-GUI SW  script editor etc? 

OR I have to code the Microcontroller board FRDM-KL25Z comes with EVBs kit, I am not sure even this is possible to do so .. 

 

 

Thanks in advance and look forward.

0 件の賞賛
返信
6 返答(返信)

4,425件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello AbdulHaleemMalik,

I hope all is great with you. Thank you for using the NXP communities.

Could you please specify the evaluation board used?

Regards,

David

0 件の賞賛
返信

4,338件の閲覧回数
AbdulHaleemMalik
Contributor I
Hello David!
Any latest on this please..
0 件の賞賛
返信

4,314件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello AbdulHaleemMalik,

Please accept my apologies for the delayed response.

Have you considered using the the Pulse tab from the GUI? It is used for double pulse, short circuit, and PWM testing. Note that the FRDM-KL25Z generates such pulses.

diazmarin09_0-1695754577530.png

 

Regards,

David

0 件の賞賛
返信

4,289件の閲覧回数
AbdulHaleemMalik
Contributor I

Hello David!

Thanks for the response, No issue at all. 

And yes I am aware of this feature of the GD. However, I am more interested in burst of pulses: I Mean to generate burst of pulses @ 1Khz for 30 seconds and then no pulses for next 30 seconds  and so on repeat this pattern...   It is shown in the screenshot below as well. 

 

Also Wondering if its possible to invoke this GUI(FlexGUI) in Matlab etc. and control some of its function indirectly? 

0 件の賞賛
返信

4,267件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello AbdulHaleemMalik,

I am pleased to contact you again.

1. I am afraid that the pulse tab only supports double pulse, short circuit, and PWM testing.

2. FlexGUI is not intended to support external firmware such as Matlab.

Please accept my apologies for any inconvenience this situation might cause.

Regards,

David

0 件の賞賛
返信

4,390件の閲覧回数
AbdulHaleemMalik
Contributor I

Hello dear! 

Thanks for the prompt response, Yes all well here. 

The Evaluation board we are using is GD3160 XM3 Half-Bridge Evaluation Kit .. Earlier we used it in our Lab for Double Pulse Test and Short Circuit as well. 

I wonder, if there is a possibility to generate the pulses at specific interval on GH/GL pins ?

 

 

0 件の賞賛
返信