Floating Outputs on MC33883

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Floating Outputs on MC33883

967件の閲覧回数
rmaryniu
Contributor I

Hi,

I am testing the MC33883 in the typical application (as shown in figure 14) and noticed that when the output of the mosfet (source of high side mosfet/drain of low side mosfet) is not connected to a load the voltage sits at Vboost - 4 and can supply enough current to drive small loads even when the inputs are low.

Is this within the expected operation of the circuit or can I modify the circuit so that the output is floating when not connected?

Thanks in advance,

Rhyse

タグ(1)
0 件の賞賛
返信
0 返答(返信)