TJA1043

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1043

624 Views
rajesh_patnaik_
Contributor I

Hello

 

Hope you are doing well!

 

Below is the 14pin High-speed CAN transceiver(TJA1043).

Q: at designing stage we placed some thermal vias for dissipation , since then our PCB is heating up . please suggest us , whether  to add additional vias   or is there any restriction ?

 

Awaiting  for your valuable reply!

0 Kudos
Reply
1 Reply

508 Views
lisettelozano
NXP Employee
NXP Employee

Hello Rajesh,

I’m afraid that you attached a picture/screenshot without success. Could you please provide it? Also, please check section 8.9 for the Application Hint AN1014 for PCB layout rules.

Have a great day,

Paulina

0 Kudos
Reply