Finding a appropriate chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Finding a appropriate chip

1,187 Views
gejx
Contributor I

I want to have a new chip which have the same bootloader and bottom-driven as the MC9S12XEP100MAG,do you have this chip?

0 Kudos
Reply
1 Reply

1,104 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately, it is not possible to use the same bootloader of the S12(X) devices for the newer family.

The 16-bits MCUs MagniV is available as the newest high voltage MCUs family. These MCUs runs directly from the 12V power supply – you don’t need an external power supply regulator.

The bootloader for this family is available below:

Simple Serial Bootloader for S12Z - AN draft 

More information about the MagniV family can be found on the NXP site:

S12 MagniV® Mixed-Signal MCUs for Automotive and Industrial | NXP 

I hope it helps.

Best Regards,

Diana 

0 Kudos
Reply