Finding a Microcontroller with USART,IIC and SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Finding a Microcontroller with USART,IIC and SPI

2,448 次查看
MWH
Contributor I

I am currently a second year computer science student. For my project I am looking for a Microcontroller which is equiped with USART,IIC and SPI. I have worked using HCS12 but it does not contain USART. I am planniing to use a GPS reciever unit MT3318 which communicate via UART. Can anybody suggest me a suitable microcontroller?

 

I am also looking for a development board. Can somebody suggest one of those too?

 

Thank you in advace.

0 项奖励
回复
3 回复数

2,270 次查看
TomE
Specialist II

MPC might be overkill for your project. These things are quite difficult to get up and running. MCF (ColdFire) might be closer, maybe a Flexis part. All of the MCF51 parts have SCI, SPI and I2C.

 

Do you really need a USART (the "S" means "Synchronous") or do you just need a UART? The SCI in the Flexis parts should do what you want.

 

For what you're making that may be overkill. You might get by with a PIC.

 

Tom

 

0 项奖励
回复

2,270 次查看
jonr
Contributor III

I agree that the MPC5634 does much more,  but if you start with the code I mentioned, then it is easy to get running.

0 项奖励
回复

2,270 次查看
jonr
Contributor III

The TRK-MPC5634 ($99) plus the code at ecu.zeeff.com might be a suitable choice.

0 项奖励
回复