MPC567xKEVB including P&E Micro debugger.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC567xKEVB including P&E Micro debugger.

1,717 Views
iggi
NXP Employee
NXP Employee

This message is posted to make the information available on the web, since there wasn't any data about the feature of the EVB kit.

 

MPC5675KEVB257/473 Evaluation Kit comes with P&E's USB QORIVVA MPC55xx/56xx MULTILINK (the blue one).

 

Use the links below as a reference.

 

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320021

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC567xKEVB


Tags (2)
0 Kudos
Reply
1 Reply

1,388 Views
jonr
Contributor III

Thanks.  If somone wants to loan me one, I will make O5E (open5xxxecu.org) run on it.

0 Kudos
Reply