Falcon Mode for IMX8MM V2 for linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Falcon Mode for IMX8MM V2 for linux

1,857件の閲覧回数
shivam_awasthi
Contributor II

Hi there NXP team, I was working in this board 1st time and I have to implement FALCON mode to reduce the boot time of my board IMX8MM V2, I have tried the example related to imx6 but not succeeded it was not able to exicute spl export command for generation of FDT. so do you have any document related to this process for IMX8MM V2.? please help me with this I have stuck on it from a long time.

and also is there any procee to launch the camera in 2-3 seconds, if is there please let me know.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,814件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please find below the document for the IMX8M family 
 
is there any procee to launch the camera in 2-3 seconds, if is there please let me know.
 
=>To launch the camera at an early stage of the boot process, one can try the below suggestions.
  • Put the required kernel module first in the makefile.
  • Put the init function at a higher level i.e early_init
Thanks & Regards
Dhruvit Vasavada
0 件の賞賛
返信

1,802件の閲覧回数
shivam_awasthi
Contributor II

Hi @Dhruvit 

Do you have any document related to this process..? if yes please share with me. 

0 件の賞賛
返信

1,774件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @shivam_awasthi,

I hope you are doing well.

Unfortunately, we have no such documents related to this.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信