Falcon Mode for IMX8MM V2 for linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Falcon Mode for IMX8MM V2 for linux

1,830 Views
shivam_awasthi
Contributor II

Hi there NXP team, I was working in this board 1st time and I have to implement FALCON mode to reduce the boot time of my board IMX8MM V2, I have tried the example related to imx6 but not succeeded it was not able to exicute spl export command for generation of FDT. so do you have any document related to this process for IMX8MM V2.? please help me with this I have stuck on it from a long time.

and also is there any procee to launch the camera in 2-3 seconds, if is there please let me know.

Tags (2)
0 Kudos
Reply
3 Replies

1,787 Views
Dhruvit
NXP TechSupport
NXP TechSupport
 
I hope you are doing well.
 
Please find below the document for the IMX8M family 
 
is there any procee to launch the camera in 2-3 seconds, if is there please let me know.
 
=>To launch the camera at an early stage of the boot process, one can try the below suggestions.
  • Put the required kernel module first in the makefile.
  • Put the init function at a higher level i.e early_init
Thanks & Regards
Dhruvit Vasavada
0 Kudos
Reply

1,775 Views
shivam_awasthi
Contributor II

Hi @Dhruvit 

Do you have any document related to this process..? if yes please share with me. 

0 Kudos
Reply

1,747 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @shivam_awasthi,

I hope you are doing well.

Unfortunately, we have no such documents related to this.

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
Reply