Facing problem while using NX3L4051 as a Demux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Facing problem while using NX3L4051 as a Demux

1,322件の閲覧回数
nileshkarale
Contributor I

Hi,

I am using NX3L4051 as a Demux, in my application there is requirement of input signal coming to input Z is having different groung than IC's ground. While enabling channel 0 (Y0) S1S2S3Ebar=0, but I have observed that there are all channels enables and whatever the input coming to Y0 same coming at all other channels. Please help me to understand that is this happening because of the separate grounds?

Thanks,

NIlesh

0 件の賞賛
返信
1 返信

1,191件の閲覧回数
Bulat
NXP Employee
NXP Employee

Unfortunately the description is not clear. Can you provide connection diagram of the NX3L4051and signal source,  and point out voltage difference between different grounds?

Regards,

Bulat

0 件の賞賛
返信