AFIC10275N-EVAL Data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFIC10275N-EVAL Data

2,641件の閲覧回数
gabrielmayo
Contributor I


I am interested in using the AFIC10275N in a new design.  Is there test data available for the evaluation board.  I am particularly interested in harmonic content at the output as well as in-band noise with no input signal.

In addition, I am targeting 200W rather than 250W output power.  Is there test data at different supply voltages?

I would appreciate any test data available on this device or eval board.

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,412件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Please create a Service request.

How I could create a Service Request?

0 件の賞賛
返信

2,412件の閲覧回数
gabrielmayo
Contributor I

Any answers?  I have an active design and I assumed that NXP would provide sport through this forum.  I also purchased  the evaluation board but it came with supporting NO documentation, not even labeling on the IO or power terminals .  The data sheet is exceptionally lacking in terms of guidance of how to bias the gates and the app notes are generic and do not claim to be applicable to this device.  In particular the datasheet does not specify the current multiplier for gate biasing of the two stages.  It does also not provide guidance in terms of drain voltage for stage 1.

Does anybody have suggestions in terms of how to get support from NXP?

0 件の賞賛
返信