FS32K144HFT0VLLT processor availability date? Pinout information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS32K144HFT0VLLT processor availability date? Pinout information

1,678件の閲覧回数
codyzimmermann9
Contributor I

When will the FS32K144HFT0VLLT processor be available to sample/purchase? Additionally, I am looking for the IO Signal Description Input Multiplexing sheet(s) attached to the Reference Manual for the same MCU. I do not see it attached to the reference manual.

Anybody able to assist with the above information?

タグ(1)
1 返信

1,519件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

microcontroller FS32K144HFT0VLLT is available at NXP website. Please check the link below:

32-bit Automotive General Purpose MCUs|NXP  

IO signal description sheet is part of reference manual. Please see the figure below:

pastedImage_5.png

If you have any other question, please feel free to write me back.

Regards,

Martin