FRDM-KL25Z source clock for UART0 in polling mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z source clock for UART0 in polling mode

Jump to solution
1,176 Views
mato_cica1
Contributor II

Hi NXP Community,

Please, what source clock should I use for UART0 in polling mode on FRDM-KL25Z?
I suppose that should be MCGFLLCLK clock or MCGPLLCLK/2. If so, which on of them?

Thanks in advance,

Labels (1)
Tags (2)
1 Solution
1,075 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Mato,

It is MCGFLLCLK. UART0 clock source could be the MCG PLL/FLL clock. You can see in to picture that there is no /2 divider in the path.

pastedImage_1.png

Regards,

Jing

View solution in original post

2 Replies
1,076 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Mato,

It is MCGFLLCLK. UART0 clock source could be the MCG PLL/FLL clock. You can see in to picture that there is no /2 divider in the path.

pastedImage_1.png

Regards,

Jing

1,075 Views
mato_cica1
Contributor II

Thanks a lot, Jing.

0 Kudos
Reply