External field detection when RF already present

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External field detection when RF already present

1,728 次查看
Bhavin-Dhulkotiya
Contributor I

Hello @KaiLi 

 

We don't want to turn on the field if the external RF field is present in PN7462. The software enables external field detection and the CLIF_ANA_NFCLD_REG = 0x0C by default though sometimes it is not detecting even if the external field is present.

1. How to set the value of CLIF_ANA_NFCLD_REG? Can you point to the document?
2. What could be the reason for not detecting sometime?

PN7462 

标签 (1)
  • RF

0 项奖励
回复
3 回复数

1,675 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Bhavin-Dhulkotiya 

I would like to know if the code and board you are debugging are from NXP? If so, which one? Because the problem you are facing now may be related to both hardware and software.

BR

kelly

0 项奖励
回复

1,673 次查看
Bhavin-Dhulkotiya
Contributor I

Hello @KaiLi

Thank you for clarifying the problem promptly.

I use a custom code and board referenced from the NXP WLC CTN730 Poller EVK.
Can you please elaborate on which block of software/hardware is affected? What do we need to configure correctly to ensure proper detection of the external field?
Can you please share the document to debug or configure related parameters?

0 项奖励
回复

1,583 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Bhavin-Dhulkotiya 

So, what you use the Demo board is OM2T730R120, right? If yes, then its design resources and reference materials need to sign an NDA with NXP to obtain.

 

0 项奖励
回复