Hi,
I have multiple BlueBox 3.0 with two different type of boards, SCH-47101 REV C and SCH-47101 REV D.
I am using the OVSP codedrop 0.8.0 image on the S32G.
With the rev C board, I can use the 1ge_P3 and 1ge_p4 port to communicate with the S32, no issues.
But with the rev D board, I can't even do a ping. The phy lights stay still when i try a ping from the CPU. But they do blink when I ping from a computer, so the PHY seems to be working.
I think it is a configuration issue between the CPU, SJA and PHY on the rev D board.
But I can't ping the SJA1110 on either board to flash it with TFTP.
What are the default configurations of the SJA1110 on the rev C and D Bluebox 3.0?
Can I flash them without using the JTAG ?
Hi,
Please submit a ticket at NXP.com, or contact FAE/sales assigned to your company in order to further assistance.
Thanks for understanding.
BR, Petr