Executing commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Executing commands

1,042 Views
tonyZ
Contributor I

Hello all, 

 

I see that in the "NTAG 424 features and hints" document there are many references to commands. Are these commands the type that would be executed in a cli? If so how do you config environment to execute commands?

 

Thanks, 

 

Tony

Tags (1)
0 Kudos
Reply
1 Reply

1,013 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir this is Fabian,

Thank you very much for contacting us.

These aren't commands that are intended to be executed directly into a CLI.

These commands are intended to be sent by an NFC Reader to the NTAG 424. We highly recommend to use RFIDDiscover for configuration of the tag and, command exchange.

These commands are part of the ISO7816-4 and ISO14443 specifications.

Additional to this, we do provide an NFC Reader Library in case you are interested in building your own application with our NFC Readers.

Best Regards,
Fabian
0 Kudos
Reply