Does the PCF85063A RTC reset the clock counting when I write a new value in the "seconds" register?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the PCF85063A RTC reset the clock counting when I write a new value in the "seconds" register?

ソリューションへジャンプ
1,301件の閲覧回数
ugobugo
Contributor I

Hello, I'm working with a PCF85063A RTC. For a sped up debug mode of my product, I want to rewrite the hour and date registers every about 2seconds. 

My question is the following. Let's say the RTC time is currently 12h 00m 00s and will switch to 12:00:01 in about 100ms. If in this moment I write a new time - for instance 13:45:30 - will the RTC switch to 13:45:31 in 100ms, or will the counting reset and the RTC will switch to 13:45:31 after 1 second?

タグ(3)
0 件の賞賛
返信
1 解決策
1,278件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

When you write a new time to the PCF85063A at any moment, the internal time base continues counting uninterrupted. It means that if you write the new time just 100ms before the next second tick, the RTC will increment to 13:45:31 in 100ms, not after a full second. The counting does not reset and there is no delay or pause after a time write.

BRs, Tomas

元の投稿で解決策を見る

2 返答(返信)
1,276件の閲覧回数
ugobugo
Contributor I

Thank you!

0 件の賞賛
返信
1,279件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

When you write a new time to the PCF85063A at any moment, the internal time base continues counting uninterrupted. It means that if you write the new time just 100ms before the next second tick, the RTC will increment to 13:45:31 in 100ms, not after a full second. The counting does not reset and there is no delay or pause after a time write.

BRs, Tomas