Does MC33FS8430G1ES has FCCU1 or FCCU2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does MC33FS8430G1ES has FCCU1 or FCCU2?

Jump to solution
3,961 Views
jingfang
Contributor IV

What pin does MC33FS8430G1ES  have? I only found the series pin definition in FS84_FS85C,but MC33FS8430G1ES is having buck3,which is different from FS8400 series.I want to use FCCU1 or FCCU2 as watchdog monitor, so I wonder if MC33FS8430G1ES has this pin?

捕获.JPG

0 Kudos
Reply
1 Solution
3,868 Views
guoweisun
NXP TechSupport
NXP TechSupport

FS85/84 WD功能都需要LFSR来获得seed,不然无法操作WD,你选择的那个SBC一样都有

View solution in original post

0 Kudos
Reply
9 Replies
3,913 Views
guoweisun
NXP TechSupport
NXP TechSupport

8430的引脚BUCK1/2/3配置跟8530一样的,FCCU and VMONX配置跟8400一样。

WD的外部监控是RSTB可以做,FS0B也可以但是要通过下面的设置:

guoweisun_0-1653868108351.png

 

0 Kudos
Reply
3,907 Views
jingfang
Contributor IV

RSTB是输出功能吧?这个目前是设计连到有中断的I/O。

EWM_OUT_b这个也是输出功能,是MCU喂狗发生错误时,告知MC33FS8430G1ES ,应该要连到MC33FS8430G1ES哪边?

0 Kudos
Reply
3,905 Views
guoweisun
NXP TechSupport
NXP TechSupport

RSTB跟FS0B 都是safety function 输出脚位,如果MCU喂狗有错误,错误会累加累加到最大值RSTB、FS0B就拉低了根据我上个回复的插图。

 

0 Kudos
Reply
3,884 Views
jingfang
Contributor IV

好的 谢谢~

但是我看规格书:LFSR有特别写在FS85,FS84是否有此暂存器?

捕获.JPG

 

0 Kudos
Reply
3,881 Views
guoweisun
NXP TechSupport
NXP TechSupport
这个寄存器是配置WD seed相关的跟FCCU关系不大啊。
0 Kudos
Reply
3,872 Views
jingfang
Contributor IV

是的,你不是说外部watchdog状态可以通过 RSTB 或 FS0B来监控,WD_ERR_LIMIT值是对比LFSR的值的结果来决定是+还是-,LFSR规格只有写在FS85,我用这个MC33FS8430G1ES,不知道有没有LFSR。

0 Kudos
Reply
3,869 Views
guoweisun
NXP TechSupport
NXP TechSupport

FS85/84 WD功能都需要LFSR来获得seed,不然无法操作WD,你选择的那个SBC一样都有

0 Kudos
Reply
3,954 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please get note that FS8430 doesn't have FCCU pins.

0 Kudos
Reply
3,940 Views
jingfang
Contributor IV

您那有文档有定义8430的引脚不,可以分享我一下么?

或者有哪个引脚可以作为MCU的watchdog外部监控?

因为该案子是匹配S32K1有EWM,我想连到MC33FS8430G1ES的引脚,作为外部watchdog监控。

0 Kudos
Reply