Does CBTL06GP213EE Support eDP singnal Switch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does CBTL06GP213EE Support eDP singnal Switch?

ソリューションへジャンプ
2,012件の閲覧回数
Makabaka
Contributor II

Dears:

Does CBTL06GP213EE support EDP signal switching?

 

I have used as DP signal switching before, but now I need to switch EDP signal.

 

Looking forward to your reply

0 件の賞賛
返信
1 解決策
2,001件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Ziv,

eDP use the same electrical signaling as DP for main data lanes.

So, yes, the CBTL06GP213 can support eDP. If you need a higher bandwidth, the CBTL06DP213 is a better option.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,002件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Ziv,

eDP use the same electrical signaling as DP for main data lanes.

So, yes, the CBTL06GP213 can support eDP. If you need a higher bandwidth, the CBTL06DP213 is a better option.

Best regards,

Tomas

0 件の賞賛
返信
1,997件の閲覧回数
Makabaka
Contributor II

Hi Tomas:

 

Yes, I've read the CBTL06DP213's specifications. It support  DP V1.3 and 8.1GBIT/S.

 

Thanks for your reply.

0 件の賞賛
返信