Does CBTL06GP213EE Support eDP singnal Switch?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CBTL06GP213EE Support eDP singnal Switch?

Jump to solution
2,030 Views
Makabaka
Contributor II

Dears:

Does CBTL06GP213EE support EDP signal switching?

 

I have used as DP signal switching before, but now I need to switch EDP signal.

 

Looking forward to your reply

0 Kudos
Reply
1 Solution
2,019 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Ziv,

eDP use the same electrical signaling as DP for main data lanes.

So, yes, the CBTL06GP213 can support eDP. If you need a higher bandwidth, the CBTL06DP213 is a better option.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
2,020 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Ziv,

eDP use the same electrical signaling as DP for main data lanes.

So, yes, the CBTL06GP213 can support eDP. If you need a higher bandwidth, the CBTL06DP213 is a better option.

Best regards,

Tomas

0 Kudos
Reply
2,015 Views
Makabaka
Contributor II

Hi Tomas:

 

Yes, I've read the CBTL06DP213's specifications. It support  DP V1.3 and 8.1GBIT/S.

 

Thanks for your reply.

0 Kudos
Reply